Product groups

KIPP presents its new catalogue at the 2018 automatica

go back

KIPP presents its new catalogue at the 2018 automatica

HEINRICH KIPP WERK will be exhibiting at the automatica in Munich, Germany between 19 and 22 June.
The company will use this event to present many new products to the visitors.
These can not only be found at the trade fair but also, to a large extent in the new OPERATING PARTS | STANDARD ELEMENTS product catalogue.

HEINRICH KIPP WERK will be presenting its comprehensive stainless steel range at the automatica 2018. Included in this will be the new product line NOVOnox hygienic. Visitors can look forward to seeing numerous new products such as cam levers, star grips, levelling feet and hinges in matt finished or polished versions.

Stainless steel T-grip

Special attention is given to the ergonomic stainless steel T-grip, that stands out with its new design and simple handling.

This classic operating grip is available in three different grip sizes with M6 to M12 internal threads and a choice between electropolished or abrasive blasted.

NEW: OPERATING PARTS | STANDARD ELEMENTS catalogue

The KIPP team will also be bringing the new OPERATING PARTS | STANDARD ELEMENTS catalogue along, this contains more than 28,000 products including 3,500 new and expanded items on its 1,350 pages.

HEINRICH KIPP WERK can be found in hall A5 at booth 408. The KIPP team looks forward to meeting all interested visitors and invites them to enjoy a Cappuccino in our own CAFÉ lounge.

Request your complimentary exhibition ticket here:

info@kipp.com

Search
Shopping cart
Number of items: 0
Amount: 0.00  
Display
Speed ordering
Availability
Here you can check item's availability.
Iran
Sitemap Print Top
Copyright © 2025 HEINRICH KIPP WERK GmbH & Co. KG · All rights reserved. Phone +49 (0) 74 54 / 793-0 · Fax +49 (0) 74 54 / 793-33